Hello Dear,
This is Jane from MirTec.
We are using DLP4500 and would like to request a design file for your reference.
Model : DLP4500(0.45" WXGA DMD)
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Dear,
This is Jane from MirTec.
We are using DLP4500 and would like to request a design file for your reference.
Model : DLP4500(0.45" WXGA DMD)
Best regards,
Hello Jane,
Welcome to the E2E forums and we hope to assist you with your questions.
If you are looking for general DLP4500 design files you can look here at the DLP4500-C350 reference design in the following link:
https://www.ti.com/tool/DLP4500-C350REF
If you are talking about the optical engine, we do not have information on that as the optical engine is not designed by TI and by iView. You will have to reach out to iView for more information about the optical engine.
Regards,
Alex Chan
Hello, Alex Chan
Thank you for your reply. I know We didn't do optical design by TI.
However, I heard from someone else that they can provide an optical engine file(ex: xx.zar ) that can be used using the panel.
If information sharing is possible, it will be helpful to compare it with the design currently used and analyze improvements.
Best Regards,
Jane
Hello Jane,
I will double check with the team but I am not aware of any optical engine .zar files.
Do you have an existing DLPLCR4500EVM and want the optical engine design for that for analysis and comparison or are you looking to create a customized optical engine design?
Thanks for your patience.
Regards,
Alex Chan
Hello Jane,
I checked with my team and we do not have the optical engine design files for the DLPLCR4500EVM as we do not design the optical engine itself.
Thank you for your time and I will close out this ticket.
Regards,
Alex Chan