This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC120-Q1: Initial brightness setting in DLPC120 firmware.

Part Number: DLPC120-Q1


Hi,

We are developing an application based on DLP3030 using Q7 RGB LEDs. 

We are facing some issue in brightness setting. In our application we setting the  initial brightness as 3277(5% in our case) but, we observed that there might be some initial brightness setting (30000) is already there in the firmware because of that  we could observe transition from 30000 to 3277 while bootup.

We want to know whether there is any default brightness is setting in TI firmware during bootup. if so, could you please provide a dlpc120 firmware with 0 as default brightness value.