Other Parts Discussed in Thread: DLPC3478, DLP3010, DLPA2005, DLPC3470
Hi
We are controlling a DLP3010EVM-LC using I2C over USB.
We like to use a mechanical switch to indicate when a moving wagon is in the correct position. Once the wagon is in position we like to start projecting a constant pattern onto the wagon. This means we either need to simply turn on the LEDs or maybe change operating mode. We don't need to entirely turn on/off power the the entire projector unit.
We like to connect the switch directly to the projector without going trough the PC. The pattern we are going to project is constant will either be streamed to the projector or have already been transferred to the projector. There are several pins exposed on the projector. What pin can we use? Where can we find the electrical documentation for this?
A diagram of what we are trying to achieve shown below.
Best Regards
Kristian