This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3479: DLPC3479: Internal Pattern Streaming mode stops displaying patterns, too

Part Number: DLPC3479
Other Parts Discussed in Thread: DLPA3005, , DLP4710

Hi TI's Friends

I'm Jia, a DLP engineer from Wintech Inc.

https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/1307967/dlpc3479-internal-pattern-streaming-mode-stops-displaying-patterns?tisearch=e2e-sitesearch&keymatch=DLPC3479#

We encounter the conpletely same problem as the friend Junfa.

Please watch the below short video

test report:

test 1: after 11 hours, one of four devices did not work, then restart all the devices

test 2: after 2 hours,one of four devices did not work, then restart all the devices

test 3: after 22 hours, one of four devices does not project patterns. with doing nothing,

test 4: after another 20 hours, the other three devices are working well now (in the video)

Hardware:

1. our custom double DLPC3749s + DLPA3005 + DLPC4710LC, the same as TI'EVM all most

2. We have produced 30 devices

3. It's a entirely random issure in different devices

Software:

1. using the V8.1 DLPC3479 firmware. TIRef-DLPC3479-DLPA3005-AC_Only-CurrentLimitsRemoved-BlueOnly-v8p1p001, shared from TI in the 2021

Trigger the patterns

1. Test 1 : as the same as the Junfa, I used IIC command to send constantly the "Run Once" command to DLPC3479 to display two pattern sets. There are random issues

2. Test 2 : I changed to send "Trigger In" signals, instead of the IIC command, from an external MSP430 MCU board. There are random issues too

3. Test 3 : I changed the pattern set pre/exposure/post time\ the number of pattern in the sets\reprogram the fireware\, but there are random issues too

4. I'm sure all the configurations to pattern set are correct

Advanced Tests:

1. when the device stoped projecting patterns. I did nothing and  I did not restart

2. I connected the usb to the device

3. I sent sorts of commands to device through the TI'GUI and all returned OK, but DMD did not display any patterns/images all the time. except DLPC3479 sent trigger outs correctly 

4. and I found illuminator LED working OK some times but DMD did not work

01/04/2024 05:41:52.3540 PM		Read System Software Version	D2	00 00 00 00
01/04/2024 05:41:59.6239 PM	I2C	Read System Software Version	D2	00 00 04 04
01/04/2024 05:42:01.4689 PM	I2C	Read Controller Device Id	D4	0C
01/04/2024 05:42:03.2355 PM	I2C	Read Dmd Device Id	D5 00	60 0D 00 8A
01/04/2024 05:42:05.0050 PM	I2C	Read Dmd Device Id	D5 00	60 0D 00 8A
01/04/2024 05:42:05.9879 PM	I2C	Read Firmware Build Version	D9	00 00 01 08
01/04/2024 05:42:07.5706 PM	I2C	Read System Temperature	D6	FF 07
01/04/2024 05:42:10.9919 PM	I2C	Read Short Status	D0	81
01/04/2024 05:42:11.8399 PM	I2C	Read Short Status	D0	81
01/04/2024 05:42:15.1007 PM	I2C	Read System Status	D1	00 04 00 04
01/04/2024 05:42:25.9839 PM	I2C	Read Operating Mode Select	06	04
01/04/2024 05:42:28.4612 PM	I2C	Read Splash Screen Select	0E	00
01/04/2024 05:42:30.6374 PM	I2C	Read Splash Screen Header	0F 00	80 07 38 04 B0 B8 00 00 02 01 01 01 00
01/04/2024 05:42:35.6512 PM	I2C	Read External Video Source Format Select	08	43
01/04/2024 05:42:38.4034 PM	I2C	Read Video Chroma Processing Select	0A	00 00
01/04/2024 05:42:41.5702 PM	I2C	Read 3 D Control	21	02
01/04/2024 05:42:44.2510 PM	I2C	Read Sequence Binary Version	9B	01 0A 01 00
01/04/2024 05:42:48.8764 PM	I2C	Read Validate Exposure Time	9D 00 00 00 00 00 00	00 C8 00 00 00 00 00 00 00 00 00 00 00
01/04/2024 05:42:52.3878 PM	I2C	Read Trigger In Configuration	91	03
01/04/2024 05:42:56.6696 PM	I2C	Read Trigger Out Configuration	93 00	01 00 00 00 00
01/04/2024 05:42:59.2242 PM	I2C	Read Pattern Ready Configuration	95	01
01/04/2024 05:43:00.3250 PM	I2C	Read Pattern Ready Configuration	95	01
01/04/2024 05:43:03.3391 PM	I2C	Read Pattern Ready Configuration	95	01
01/04/2024 05:43:04.1167 PM	I2C	Read Pattern Configuration	97	02 07 04 88 13 00 00 F4 01 00 00 64 00 00 00
01/04/2024 05:43:06.5550 PM	I2C	Read Pattern Configuration	97	02 07 04 88 13 00 00 F4 01 00 00 64 00 00 00
01/04/2024 05:43:07.2207 PM	I2C	Read Pattern Configuration	97	02 07 04 88 13 00 00 F4 01 00 00 64 00 00 00
01/04/2024 05:43:07.7963 PM	I2C	Read Pattern Configuration	97	02 07 04 88 13 00 00 F4 01 00 00 64 00 00 00
01/04/2024 05:43:08.0180 PM	I2C	Read Pattern Configuration	97	02 07 04 88 13 00 00 F4 01 00 00 64 00 00 00
01/04/2024 05:43:13.8612 PM	I2C	Read Look Select	23	00 00 01 00 00 00
01/04/2024 05:43:16.3134 PM	I2C	Read Sequence Header Attributes	26	00 00 00 00 00 64 AD DE 04 00 10 A2 03 00 0C 00 00 00 00 00 64 AD DE 04 00 10 A2 03 00 0C
01/04/2024 05:43:22.8535 PM	I2C	Read Led Output Control Method	51	00
01/04/2024 05:43:24.3269 PM	I2C	Read Rgb Led Enable	53	04
01/04/2024 05:43:25.0029 PM	I2C	Read Rgb Led Enable	53	04
01/04/2024 05:43:25.4165 PM	I2C	Read Rgb Led Enable	53	04
01/04/2024 05:43:25.5780 PM	I2C	Read Rgb Led Enable	53	04
01/04/2024 05:43:25.7497 PM	I2C	Read Rgb Led Enable	53	04
01/04/2024 05:43:26.4856 PM	I2C	Read Rgb Led Current	55	32 00 32 00 32 00
01/04/2024 05:43:27.0088 PM	I2C	Read Rgb Led Current	55	32 00 32 00 32 00
01/04/2024 05:43:27.2714 PM	I2C	Read Rgb Led Current	55	32 00 32 00 32 00
01/04/2024 05:43:27.9476 PM	I2C	Read Rgb Led Enable	53	04
01/04/2024 05:43:29.2901 PM	I2C	Read Caic Led Max Available Power	57	D5 38
01/04/2024 05:43:29.8946 PM	I2C	Read Caic Led Max Available Power	57	D5 38
01/04/2024 05:43:31.7276 PM	I2C	Read Rgb Led Max Current	5D	FF 03 FF 03 FF 03
01/04/2024 05:43:33.2007 PM	I2C	Read Caic Rgb Led Current	5F	00 00 00 00 00 00
01/04/2024 05:43:35.1888 PM	I2C	Read Caic Image Processing Control	85	00 20 00
01/04/2024 05:43:41.7755 PM	I2C	Read Flash Update Precheck	DD 00 00 00 00	00
01/04/2024 05:43:46.5625 PM	I2C	Read Input Image Size	2F	80 07 38 04
01/04/2024 05:43:47.9849 PM	I2C	Read Display Size	13	00 00 00 00
01/04/2024 05:43:48.9873 PM	I2C	Read Display Size	13	00 00 00 00
01/04/2024 05:43:49.9267 PM	I2C	Read Display Image Orientation	15	00
01/04/2024 05:43:51.9629 PM	I2C	Read Display Image Curtain	17	00
01/04/2024 05:43:52.5174 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:53.0219 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:53.2237 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:53.5979 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:53.7895 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:53.9914 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:54.1530 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:54.3350 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:56.6846 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:57.8769 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:43:58.5227 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:00.6201 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:01.1554 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:01.6703 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:03.5632 PM	I2C	Write Image Freeze	1A 01	
01/04/2024 05:44:05.8055 PM	I2C	Read Image Freeze	1B	01
01/04/2024 05:44:06.9360 PM	I2C	Read Image Freeze	1B	01
01/04/2024 05:44:07.7819 PM	I2C	Read Image Freeze	1B	01
01/04/2024 05:44:09.2155 PM	I2C	Write Image Freeze	1A 00	
01/04/2024 05:44:09.7604 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:10.2969 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:10.7411 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:11.0644 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:11.3750 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:11.7558 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:14.5815 PM	I2C	Read Border Color	B3	00
01/04/2024 05:44:15.0380 PM	I2C	Read Border Color	B3	00
01/04/2024 05:44:15.2610 PM	I2C	Read Border Color	B3	00
01/04/2024 05:44:15.4612 PM	I2C	Read Border Color	B3	00
01/04/2024 05:44:16.0171 PM	I2C	Read Border Color	B3	00
01/04/2024 05:44:16.1786 PM	I2C	Read Border Color	B3	00
01/04/2024 05:44:19.0654 PM	I2C	Read Image Freeze	1B	00
01/04/2024 05:44:20.7503 PM	I2C	Read Display Image Curtain	17	00
01/04/2024 05:44:21.8993 PM	I2C	Read Display Image Orientation	15	00
01/04/2024 05:44:23.0251 PM	I2C	Read Display Size	13	00 00 00 00
01/04/2024 05:44:24.1450 PM	I2C	Read Display Size	13	00 00 00 00
01/04/2024 05:44:24.8311 PM	I2C	Read Input Image Size	2F	80 07 38 04
01/04/2024 05:50:30.4425 PM	I2C	Read Sequence Binary Version	9B	01 0A 01 00
01/04/2024 05:50:30.9347 PM	I2C	Read Sequence Binary Version	9B	01 0A 01 00
01/04/2024 05:50:31.1352 PM	I2C	Read Sequence Binary Version	9B	01 0A 01 00
01/04/2024 05:50:31.3158 PM	I2C	Read Sequence Binary Version	9B	01 0A 01 00

We all know DLP4710\3010\2010 have the same issues

But Fortunately, the latest fireware V9.0 to 3010/2010 has fixed the known issues

Please let me know if you have any good news

myTi's ID : jiawq@dspchina.com

Thank you for any help

Best Regards

Jia