Dear all,
I'm trying to use an E4750LC with an DLPC3479 display and light controller to display a simple pattern. Unfortunately when I try to do it I can't see the clear image, I see only vertical and horizontal bars alternating each other and then it stops. When I click the Run continuously it is having the same behaviour. When I click stop, I see a bar, but alway in another place.
Could you please advice me on what could be the issue?
A second question is what is the max Exposure time that could be set? In this case also if I change it, it stays the same.
Thank you,
Raffaele