Other Parts Discussed in Thread: DLPA3000,
Hi ti experts,
I have a custom DLPC3478 board with DMD3010 and DLPA3000. I have STM32 on our DLPC board to upload DLP firmware and control the DLPC3478 through I2C.
I discovered that, in Internal pattern mode, with mono or rgb color, if we set pre and post exposure times to 15 ms and exposure time to anything lower than 11 ms, projector is not projecting in firmware version v9.0.1. However, if we switch into firmware version v8.0.1, it is working with the same exposure times (for example 15 for pre exp, 10 for exp, 15 for post exp).
Can you help us with this issue?