This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR65EVM: inquiry for repair

Part Number: DLPLCR65EVM
Other Parts Discussed in Thread: DLPC900

TI E2E Support,

 DLPLCR65EVM seems it is broken which we purchased last September. I would appreciate it if you could let me know the way to fix this.

  1. DLPC900 GUI shows 1)Controller/DMD Incompatible, and 2)DMD Micromirror Parked.
  2. Here are the information of Serial communication log:

Debug opened on URT0
Memory test cc = 1
API version: 06.02.00
App version: 06.02.00
Configuration layout versions:
     Seq Map: 90.00.0001
     SW Map: 90.00.0000
Bootloader Version 4.2.0
Jumping to application ...
Debug opened on URT0
Memory test cc = 1
API version: 06.02.00
App version: 06.02.00
Configuration layout versions:
     Seq Map: 90.00.0001
     SW Map: 90.00.0000
I2C Cmd Secondary Address 34
digcontrol_init complete: 1
thinapp : Goto State : 3 0
DRAM memory pool 0010F1E8 2000F1E8
Autolock initialization passed
Picture Control: Default System Mode 0
thinapp : Display mode 1 0
Displaying Video Curtain...
Illumination: Transition to operating mode
DMD comm error in DMD_Power()
Illumination: Disable Illumination
Illumination: Transition to Standby Mode complete

3. voltage measurement of DLPLCR65EVM

  • DMDP3P3V: 3.3V
  • EN_OFFSET: 0V
  • VOFFSET (TP20): 2.96V (regularly 8.5V)
  • VRESET (TP21): 0.148V (regularly -10V)
  • VBIAS (TP33): 0.2V (regularly 16V)

Finally, here is the purchase order.

42.pdf

Thank you for your cooperation.