Other Parts Discussed in Thread: DLP3010, , DLPA2005
Hello.
I am using a custom board using DLPC3478+DLPA2005+DLP3010.
The DLP FW originally used was 7.4.2 and the GUI was 3.1.0.6.
Using the DLP EVM GUI,
An internal patterns index was configured, a Pattern Data File (.bin) was created, an img was created through Edit firmware, and the created img was updated.
The above process was followed and was used normally.
After updating the firmware, the pattern was output normally when run continuously in internal pattern mode.
In the meantime, I changed the FW version to 9.0.1, used the same Flash firmware, and ran it in Run continuously in Internal pattern mode.
The pattern is output only once and then stops.
(When I check Read Pattern Order Table Entry and Read Internal Pattern Status in Advanced mode-> Light control, the Pattern Data file information I entered appears.)
The important thing here is,
Except for the flash image being changed from 7.4.2 to 9.0.1, all conditions are the same.


Are there any changes in that part as the Flash image version changes?
Additionally, the reason for changing the Flash image version is that when executed or repeated using an internal pattern, DLP communication becomes abnormal over time (more than 2 to 3 hours). This symptom persists until the device is completely powered off and on.
Please let me know if there has been an issue with this symptom and the history and solution.