Other Parts Discussed in Thread: DLP2000
Hello TI,
I'm using the DLPDLCR2000EVM + BBB (Debian AM335x 11.7 2023-09-02 4GB microSD IoT + bbb.io-kernel-5.4-ti-am335x) combo for synchronized pattern projection with a fast camera and I was able to achieved that but with a frequency limitation.
In this case I've used i2c command "i2cset -y 2 0x1b 0x1E 0x00 0x00 0x00 0x01 i" to enable source synchronization achieving only around 23.5 Hz and never 60 Hz.
I've manually installed DLPDLCR2000-00A0 cape from bb.org-overlays repository and also tried to change manually the "display-timings" section according to the resolution and frequency of the screen.
What am I doing wrong?
Thanks you,
Best regards,
Simone