This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3021-Q1: Flash Alternative Solution

Part Number: DLP3021-Q1

Dear Team,

We're planning to use GigaDevice's 1G Flash (GD55LX01G). The FAE mentioned two differences between the 1G and 2G versions. Will these affect FPGA applications?

  • Chip Erase time: 100s typical (1Gb) --> Chip Erase time: 200s typical (2Gb)
  • Table of ID Definitions: C8 68 1B FF(1Gb) --> C8 68 1C FF(2Gb)

Regards,

Johns