This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9500: Is there a curve of operating temperature-lifetime?

Part Number: DLP9500

Tool/software:

Hello,

1. Is there a curve of operating temperature-lifetime if ignoring other factors. And any information of DMD lifetime under different temperature.

2.  Illumination Source Between 400 nm and 420 nm, What's problem will be occured if Illumination is out of range 11W/cm2, 26.6W.

3. Can the micromirror be damaged if Illumination is out of range, but temperature is OK.

Thanks!