I am considering a purchase of the DLP LightCrafter 9000 Evaluation Module for use in a stereolithography 3D printer. My current setup involves communicating with a DLP chip on a developer board via HDMI. The board is hooked up to the computer and windows detects it as a second monitor exactly as it would if it were a normal projector. The LabView program then uses a folder of previously created black/white images and "full-screens" them on the second monitor at different intervals during the printing process. Would the 9000EVM be able to work in a similar way or are there no LabView libraries that can communicate with the 9000EVM? This would present a great advantage to us as the newer DLP provides significantly higher resolution. Please let me know if any additional specs would help. Thanks!