Hi all,
does any one know the type of the dc connectors for DLP Pico Projector Kit 2.0? What is the inside and outside diameters for the dc connector? I did not find in the manual but after comparison between the one together with 5V ac adapter and the attached image(http://en.wikipedia.org/wiki/File:Photo-RoundPowerConnectors.jpg) below, it seems to be the one inside the red circle. Could some one confirm this and tell me the exact parameters(inside and outside diameters)? Thanks in advance!