Hi,
(following was carried out completely in 'pattern sequence' mode with 8-bit patterns, color as 'white', frame time 15000us, exposure time 10000us)
I am using firmware v3.0 with Lightcrafter v3.0. When I select 'PLAY ONCE' radio button, 'SEND' and 'VALIDATE' a pattern and press 'PLAY', the pattern plays once and stops. When I press 'PLAY' again, nothing shows on the projector.
But this works fine in 'REPEAT' mode: I select, 'REPEAT' mode, 'SEND' and 'VALIDATE' a pattern and press 'PLAY', the pattern sequence plays out repetitively until I press 'STOP' and I am able to play again without a problem.
Due to this problem, I had to opt out to use firmware 2.0 with Lightcrafter v2.0 which solves the problem with 'PLAY ONCE' but it does not allow me to use Variable Exposure control. (I tried using Lightcrafter 3.0 on firmware 2.0, but variable exposure control has some issues...).
May I know whether this is a common problem to all? Or am I doing something wrong and if so, how to correct it...?
Thanks in advance for the help.