Dear Mr/Ms,
I was trying to write a small program for testing with DLP@Discovery 4000 Kit. I want to display an image which is half white and half black. This means the 32-bit data bus will be writen all 0 for the first 8 clocks(16edges) and all 1 for the last 8 clocks(16 edges) in a row cycle. For a simulation it is as I have designed,but when I finished configuration, there is a problem.On the right half which should be "1" state, there are two thin straight lines ,quite obvious. Well, I can not find where the problem is. How could this happen? What do we need to care when we write the data bus ? Thank you for your attention.