Other Parts Discussed in Thread: DLPC2607
After connecting the EVM to the power i would see the default screen when no other device is connected.
Today on connecting, the D3 light stays on. and nothing around it seems to work. despite connecting it to a beaglebone or a raspberry pi cannot see an image whatsoever.
upon removal of the optical module and insertion into another EVM it seems to work.
The i2c seems to work as i can detect and set i2c. any troubleshooting mechanisms?
Also is there a possibility to purchase a replacement board without the optical module.