Other Parts Discussed in Thread: DLPA1000, TIDA-01473
Hello,
I have two separate questions:
1. I would like to use the DLPDLCR2000EVM without the light engine. I know the DLP2607 is set up to not boot without the light engine installed. However the only connection between the light engine and the controller board is a single flex cable. Is is possible to modify the board/flex cable connector so that it doesn't need the light engine plugged in to boot? For example could I short a couple of the pins (based on your recommendation) on the connector for the flex cable so that the DLP2607 thinks the light engine is still installed?
2. Is is possible to get a custom DMD flex cable (the one that connects the DMD chip to the controller board) with a different length?
Thanks,
Rusha