Dear TI,
I would like to update the DLP4710EVM-G2 firmware with the max. 12000/16000/16000 mA current setting.
Tool used: DLP LightCrafter Display EVM 7.0 (standard / advanced mode )
OS: Windows 10 , 1803
The Normal mode GUI is only let me enable to set the max current value to 12000 maA for Red/Green/Blue LEDs. ( 16000 for Green & Blue ??? )
I tried to update the stock fw ( dpp3439-dual-ASIC_1.6.0.img) with the 3x12000 mA setting, but the uptade faied with the following:
- Flas Image Update Failed : Errors updating the output image !
I got from TI the (dpp3439-dual-ASIC_1.6.266.img >> 720p/120Hz support ) , but I got the following error :
- Flash Image Update Failed: Input flash image errors !
- Flash Image Update Failed: Contact TI Application Engineer !
The I2C communication is working fine between the DLP & PC. I can set the current values manually.
I have to use the 720p with 120 Hz and as much as possible output Lumen. ( LED current ).
Best Regards
Tibor