This should be really simple. For years I had an install with CCS 3.3 and DSK5510 working with no issue. I have had to move PCs and installed CCS6 on Windows XP (no option of upgrading atm).
I have plugged the DSK5510 in and run the diagnostics to check the driver (from spectrum digital) is installed. Everything works OK. I then ran CCS 6.0.1, selected C551X and DSK5510, create a new project and compiled. Switched into debug but all the options under run are grayed out.
I have spent hours trying to work out whats wrong but theres simply not enough debug output to understand the problem.
Then I click on DSK5510.ccxml and try to work out if theres a connection problem, the test connection is grayed out. Ive tried every emulator option in the list but I know its supposed to be "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator"
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0">
<instance XML_version="1.2" desc="Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0" href="connections/SDDSKUSB_Connection.xml" id="Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0" xml="SDDSKUSB_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0">
<instance XML_version="1.2" href="drivers/sdgo5510dsk.xml" id="drivers" xml="sdgo5510dsk.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="DSK5510_0" href="boards/dsk5510.xml" id="DSK5510_0" xml="dsk5510.xml" xmlpath="boards"/>
</platform>
</connection>
</configuration>
</configurations>
When I move into debug mode and click debug, it looks for the emulator and reports Error initializing emulator
It would be really nice if SOME debug could be displayed... ANYTHING! I know the device is working, Im setting the emulator to what is suggested. Ive compiled the code and switched into debug... what more can I do?
Please can someone give me some clue as to why this is not working. I know its an older DSK but the device is used in so many products; has someone tested this?