This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDX5535EZDSP: Code Composer will not connect to the board and has issues connecting to libraries.

Part Number: TMDX5535EZDSP

Tool/software: Code Composer Studio

Hello,

We are having issues with Code Composer not connecting to the board. We have reinstalled Code Composer on two separate computers (one running Windows 8 and the other Windows 10) and the software still displays connectivity errors. The error message displayed is as follows:

"Error connecting to the target:

(Error - 600 @ 0x0)

A required dynamic library could not be located.

The library isn't on the search path.

(Emulation package 7.0.48.0)"

Thank you for your asistance.