This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in DM355 documentation?



Two different documents for DM355 mention different addresses for the same register.

In "Video Processing Back End Reference Guide", page 49 (section 3.1.1.4) the address for VPSS_CLK_CTRL is said to be "0x01C70004". 

In "ARM Subsystem User's Guide", on page 122 (section 9.10, System control registers) the offset for VPSS_CLK_CTRL is 0x44. According to Table 4-2 (ARM Configuration Bus Access to Peripherals) the address for that register should be 0x01C4:0000 + 0x44, which makes it 0x01C4:0044.

Is that an error in VPBE Guide?