I am working on a project which will use AM3784 to capture video from VIP0 and display it on HDMI output. This project will use our own decoder instead of TVP7002, which can receive PC graphic signal via VGA interface and output video data in RGB-888 format. According to AM387x technical reference manual, AM3874 should support RGB-888 input on VIP0.
To evaluate video capture performance and quality, I am trying to do a demo by using DM814x EVM board with Expansion I/O BOARD-REVD to capture 720p@60 video from VGA interface and display on HDMI output. I am currently using EZSDK-5.04.00.11. Following is what I wan to achieve.
- Configure TVP7002 selecting VGA input, bypassing color-space-conversion, output video data in RGB-30bit format.
- Configure DM814x to receive RGB-24bit data on VIP0.
- run modified example application saLoopBackFbdev.c to capture video from VGA interface and display on HDMI output.
Have anyone done this or similar test? If yes, can you please share your patch with me? If not, any idea on how to configure on both TVP7002 and DM814x side?
Any help will be highly appreciated.
Yong Zou