Other Parts Discussed in Thread: AM3892, DAC7512, PMP, TPS65010, TPS65910, BQ24022, LP3971, LP3972, TPS65023, TLV320AIC23B, TVP5150, TVP7002, THS7303, DA8XX
Hello,
I have custom board, based on TI am3892 processor. I managed to load Linux kernel + Arago FS on it.
The board's design is very similar to DM816x/CA816x/AM389x EVM but there are some valuable differences. For example we use other ethernet physics.
There is no driver for our ethernet in EVM's linux kernel config.
Could you provide some kind of guide how to install ethernet driver?
Another question is to execute HDMI video output. Which linux kernel modules should I additionally install? Syslynk, vpss? Could you also provide any guide?
The last question is about NAND. There is there nand chips on board, each has it's own chip select. By default we see only one nand device (in u-boot).
How to connect two other nand chips?
Best regards,
Anton