This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 eXperimenter Kit vs. OMAP-L138 eXperimenter Kit for Universities

Expert 2370 points
Other Parts Discussed in Thread: OMAP-L138, OMAPL138, TMS320C6748, ADS5282EVM, ADS5282

Hi,

Is 4.3” LCD the only difference between OMAP-L138 eXperimenter Kit and OMAP-L138 eXperimenter Kit for Universities ?

Both of them doesn't have flash, how can we boot them for standalone system for example ?

Apart from this breakout board for uPP extension which is not currently available, is there any other expansion connector for uPP to be used with eXperimenter or University kit ?

http://createnewstuff.webs.com/breakoutboardomapl138.htm

Thanks.