TI-API: quote: status codes in the test environment

Part Number: TI-API

Tool/software:

After submitting a quote request in the test environment the resulting quote has always quoteStatus Accept and status Pending (only exception so far: When using a customQuoteNumber more than once the quoteStatus will be Reject and the status No bid). Same thing for quote retreive calls, only that status is Bid instead of Pending. Would it be possible to introduce some test part numbers resulting in different status codes (and ideally one with a delayed transition from Pending to Bid as well) to test our workflows? And is it possible to clean up the existing quote numbers in order to use test cases more than once?

**Attention** This is a public forum