Part Number: PCA9306
Hi team,
My customer would like to use this part in the following configuration, and I have 2 questions regarding it-
'
VREF1: 1.8VDC
VREF2: 2.8VDC
I want to use the enable pin to control the state of level translator. Can I use a 3.3VDC GPIO control on enable when my VREF2 is 2.8VDC or do I have to level shift the control signal?
I know that the control voltage is within the absolute max voltage rating for the enable pin but is the voltage somehow linked to VREF2?
"
1. I don't believe they can use the 2.8V on the VREF2, if they have 1.8V at VREF1 I think they can only have VREF2 at 2.5-V, 3.3-V, or 5-V. Not 2.8V. Can you confirm?
2. Everything I am seeing on E2E looks like they cannot have separate voltages at VREF2 and EN, they must be connected and have the resistor at that connection. Can you confirm that as well?
Thanks,
Lauren