This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: DP83869HM and ONET4201LD/PA

Part Number: DP83869HM
Other Parts Discussed in Thread: ONET4201LD, ONET4201PA,

Hello,


I am using a DP83869HM with a ONET4201LD (for emitting) and a ONET4201PA (receiving) to send data with fiber. I have some questions :

- Should I place some termination resistance (100ohm or pull up) or all is included in the IC ?

- Is the ONET4201LD usable with frequency below 1Ghz ? (to do some test at 10Mbps)

- Which configuration should I use with the DP83869HM ? SGMII to copper mode, or Fiber mode ? (1000Base-T to 1000Base-X)

Thank you !