Part Number: DS90UB948-Q1
Hello,
Please see attach file for Fisker/Foxconn circuit review
Thanks
YT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zoe, Foxconn ask will 1280x52 resolution is too low for 924? Since CLK rate only 4MHz if frame rate use 60Hz
Hello YT,
924 has a minimum PCLK rate of 5MHz. Please make sure to include blanking into your calculation for frame rate here as 4MHz sounds like it is calculated only using the active dimensions of the video. But is your question about 924 or 948? Because the schematic above looks like it is for 948.
Best Regards,
Casey
Hi Casey, Foxconn ask 1. if our setting "LSB" means JEDIA format, and "MSB" means VESA format? Dose our understand is correct? 2. For the video setting shall we follow source side video format? Thanks! YT
Hello YT,
Here is a table to help decode the MAPSEL settings:
|
|
24 Bit Mode |
18 Bit Mode |
|
MAPSEL = H |
OLDI/SPWG/VESA |
4 Lane 18 Bit Mode |
|
MAPSEL = L |
JEIDA |
Standard 18 bit |
Best Regards,
Casey