Other Parts Discussed in Thread: HD3SS3212
Hello Experts,
How to design for AC coupling when HD3SS3212-Q1 for DRD application? AC coupling should place between device and USB Type-C connector, correct?
Best Regards,
Fujiwara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Experts,
How to design for AC coupling when HD3SS3212-Q1 for DRD application? AC coupling should place between device and USB Type-C connector, correct?
Best Regards,
Fujiwara
Fujiwara-san
AC coupling requirement is separate from the DRD application. For AC coupling, please refer to Figure 4, 5, 6, and 7 for the different placement option.
I would place the AC coupling cap between the HD3SS3212 and the Type-C connector as long as the source common mode voltage is between 0-2V.
AC coupling caps on TX is typically 0.1uF or 0.22uF. AC coupling caps on RX is optional 0.33uF.
Thanks
David