Part Number: DS110DF111
Other Parts Discussed in Thread: DS110DF1610
Hi team,
Could the DS110DF111 be used as a 1:2 mux / 2:1 mux, and could the DS110DF1610 be configure as 1:4 mux / 4:1 mux?
From the datasheet, if I understand correctly, they should be able to do 1 input with multiple output modes?
Could we have multiple input, and select whichever input to a single output (ie, switch between CH0 and CH1 input to CH0 output)?
If it could be done, will it route ethernet packets from the selected channel while the input packets from the not-selected input channel will be dropped, or it is capable to store the packets of the not-selected channel first and passes the packets to the output when it become the selected channel?
Regards,
SK Loo