Hi Sir,
When I was debugging the TUSB544, I found that the signal cannot be output after passing through the TUSB544. Then I compared the same products and noticed that there is signal output without adding TUSB544. By checking the Log I learned that the product can be set to adjusting the bandwidth state.
Therefore, I think if TUSB544 does not increase the gain and let the signal pass directly, this problem may be solved. So I don’t want to do EQ enhancement and pull down both DEQ and UEA ground with 1KΩ resistor. The schematic is as follows,
I was wondering if my approach is feasible? Or you can give a better suggestions to solve the problem of no signal output.
Thanks,
Best Regards