This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP149: Using SN65DP149 as DVI input stage

Part Number: SN65DP149
Other Parts Discussed in Thread: TMDS181, TMDS171, TMDS261B, TMDS361B

We are currently designing a video processing product and chose the SN65DP149 as a DVI input stage in front of an FPGA. The signal path is designed to be:

PC DVI/HDMI output -> cable -> connector -> SN65DP149 -> 100 ohms PCB traces -> FPGA I/Os.

The application example in SLLSEL2C (figure 28) shows the case of using the IC as an output stage. Unfortunately the other use case ("dongle application") is not shown, as figure 29 is a duplicate of figure 28.

Can you tell me if the IC can be used for our planned application, as described above? Do you have access to the correct schematic for the "dongle application"?

Thank you in advance.

Best regards
Lukas