Part Number: TLK10022
Hi,
Is it fair to say if we only use the TX side of the chip (aggregator only) then power consumption will be cut in half, 0.95W instead of 1.9W?
and if we run it at lower speed than 10Gbps would the power be almost cut accordingly, considering the static power consumption? i.e. about 1.6W at 7.5Gbps instead of 1.9W?
Thanks, Reza