This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Does TI have design guideline for eDP of SN65DSI86-Q1? Does it has description maixmum length of eDP lane?
Thanks
Hi:
Q1.Is eDP output 5.4Gbps for four lanes or 5.4Gbps per lane?
Page 1 of datasheet (SN65DSI86-Q1) that has description displayport with up to four lanes at either 1.62 Gbps, 2.16 Gbps, 2.43 Gbps, 2.7 Gbps,
3.24 Gbps, 4.32 Gbps, or 5.4 Gbps.
Page 5 of datasheet (SN65DSI86-Q1) that has description displayport Lane 0 transmit differential pair. Supports 1.62Gbps, 2.16Gbps, 2.43Gbps, 2.7Gbps, 3.24Gbps, 4.32Gbps, and 5.4Gbps. All DisplayPort lanes transmit at the same data rate.