This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I: DP83848I Design and Debug problems

Part Number: DP83848I

My customer has met with a problem in designing with DP83848I.

Here is the main informations about it.

1.At first, Sample A did not work properly,my customer found that it can run properly when  connect pin18 / 23 / 37 with wires during debugging;

2.The above problems have been changed on Sample B, but nothing else has changed, but it  can not work properly.

3. ABA test has been done with three Sample B  boards, and the phenomena are the same. The specific phenomena are as follows(here are schematic diagrams for Sample A and Sample B):

    (1)After the whole machine is powered on, H3 will be on immediately and normally; After a period of time, H1 turns on, and after H1 turns on, the PHY chip starts to heat, and H2 does not turn on all the time.

    (2) Add the phenomenon: H3 is always on immediately after power on, H1 / H2 is not on all the time, and PHY chip will also heat up.

Please help sovle it.Thanks a lot.