Part Number: TCA9554
Hi team,
My customer plan to use TCA9554 at 1.8V VDD and have a few questions.
- As I understand standby mode is entered automatically when there is no transaction on I2C. What is the state of I/Os during standby?
- What is the current consumption if the I/Os are set to output and tristate ? It is not clear in the datasheet.
- Why is the current consumption much higher when i2c=0khz and Vi=0 and I/Os are set to input? Is it assuming internal pull ups enabled? What is the current consumption internal pull ups are disabled and Vi=0
Thanks,
Connie