@Chuck Branch
Please generate Patch for this setup:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tomas,
Chuck is currently out of office but will help you with this configuration when he returns next week.
Is there a reason you are not able to use those configurations and download the binary?
Thank you,
Hari
Update on this? This is ridiculous...
Tomas,
We are working through the last set of issues on the Web GUI, and I will complete this configuration for you this weekend.
Regards,
Chuck
ToTomasManno.binmas,
Attached is the configured full flash binary that matches your project request.
I have to copy values from a calculator, so it is possible that I have made transposition errors. If something is wrong, please let me know and I will correct it.
Regards,
Chuck
Thanks! Is the full flash necessary? Do you have the lowRegion binary? We never got our driver to work with the full flash patching, only with the lowRegion binary.
We get this error with fullFlash binary:
acFailCode 0x01:
AC_FAIL_WRONG_HEADER_VERSION: The header
version is expected to be 1 and was not.
Tomas,
I apologizeTomasManno_LowRegion.bin. I didn't recognize that you were using a MCU boot. Attached is the low region binary that you will require.
The fullflash binary is not compatible with the PBM flow.
Regards,
Chuck
Thank you, charging works with this fix. Not too happy about the 3 month fix time though...
Tomas,
I understand the frustration. I will post a FAQ when the Web GUI is finally released.