Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Hi Team,
We are using DP83869 into our design which can operate in following modes-
– Media Support: Copper and Fiber
– Media Conversion Between Copper and Fiber
– Bridge Between RGMII and SGMII
We are using DP83869HMRGZR as media converter between Copper and Fiber (100BASE-T to 100BASE-Fx) into our design. We have connected LEDs at LED_1 and LED_2 pin of DP83869 for indication purpose. From datasheet I found that LEDS_CFG1, LEDS_CFG2 and LEDS_CFG3 resistor can be use to configure the funcnality, polarity and blink rate of the LED pins (LED_1 and LED_2). Whatever is mentioned into table 43, 44 and 45 of the datasheet is valid for all modes of operation? If not then what will the funcnality of LED_1 and LED_2 pins of DP83869 into media converter mode: 100BASE-T to 100BASE_Fx?
Best Regards,
Aditya Kumar Singh