Part Number: TPS25750
Other Parts Discussed in Thread: BQ25731, BQ25792
Hello TI,
I am working on TPS25750 for my BMS, I am expecting that TPS25750 can sink power from input wall adaptor without any configuration at initial state, is it possible ..?
Currently i am working on TPS25750 application circuit, but it's not working as per the application requirement.
I am expecting,
1. when wall adaptor(100W) is present, TPS25750 sink the 60W power from it without any configuration.
2. After the TPS25750 configure from Host controller, need to take maximum power from wall adaptor when the system required.
3. TPS25750 can support in running configuration changes, means if the tps25750 is configure and working 60W and i want make changes in TPS25750 configuration for 100W, is it possible..?
Thanks and regard,
Rahul