This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
In DS10BR150, both 100Ω Input termination and 100 Output Termination are integrated。 but for DS90LV001, there is no any in-chip termination.
Is it means that both external 100 input termination and 100 output termination must be added in design for 500MHZ LVDS signal?
Hi,
A termination resistor is required only on the input. It should match the characteristic impedance of the transmission line (90Ω to 110Ω).
Thanks
David
David;
why is a 100 output termination integrated in DS10BR150, but 100 ohm output termination is not needed in DS90LV001?
Hi,
The output resistor on this part helps to match the output impedance with the transmission line impedance. This is necessary for good transmission characteristics.
Thanks
David
I am confused with below message. does below comments mean that adding 100ohm output termination on DS90LV001 is preferred?
The output resistor on this part helps to match the output impedance with the transmission line impedance. This is necessary for good transmission characteristics.
Hi,
Internal 100-ohm resistor provides back termination. This back termination, with the100-ohm termination at the receiver, and the controlled trace impedance, provide optimum signal conditioning from signal integrity point of view. Otherwise there could be reflection - due to impedance mis-match.
On the other hand, a normal buffer, such as the DS90LV001 would operate at a much lower data rate and thus meeting tight impedance controlled environment is not a concern as much, so you do not need 100ohm termination at its output.
Thanks
David