This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
In TMUXHS412 data sheet, its application :
8.1 Application Information
The TMUXHS4412 is an analog 4-channel high-speed mux/demux type of switch that can be used for routing
high-speed signals between two different locations on a circuit board. The TMUXHS4412 can be used for many
high speed interfaces including:
In above application, no HDMI mux/demux mentioned, Is it used to mux or demux HDMI2.0 interface?
Thanks!
Hi,
For HDMI2.0, please use the HD3SS215 or the TS3DV642.
Thanks
David
Hi,
HDMI is a 3.3V DC-coupled interface, so its common mode voltage is 3.3V, outside the TMUXHS4412 common mode voltage range.
The TMUXHS4412 also does not provide muxing of HPD, DDC, or CEC bus.
So from electrical and design implementation perspective, the TMUXHS4412 will not fit a HDMI design requirement.
Thanks
David
Dear Sir,
I also have a question :how to mux、demux ac-coulpled or dc-coulpled high speed differential signal, for example, DP is ac-coupled ,but hdmi is dc- coupled.
I can understand that MUX/demux ic can mux or demux dc-coupled signal, all signal level, positive and negative signal, are above 0 zero voltage,but ac-coupled signals, is common mode voltage is zero voltage. How can the negative signal pass the MUX/DEMUX ic?
Thanks.
David
Hi,
I put together couple slides to explain the MUX AX-coupling, does this help?
Thanks
David