This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA39306-Q1: Is it suitable for 1.8V on both side, each 1V8 may power off or power on?

Part Number: TCA39306-Q1
Other Parts Discussed in Thread: TXS0102-Q1, SN74LVC2G66, TCA39306, SN74LVC2G66-Q1, TS5A3166-Q1

Hi Team

I am looking for a 1V8 I2C isolator chip to isolate two 1.8V power domain (I2C resistor pullup to) for automotive application.

Voltage on both side may be un-powered separately.  I2C speed is FM+.

There isn't a requirement of GPIO control. If any power is absent, I2C is disconnected and no current leakage will happen.

Is TCA39306-Q1 suitable for this scenario?

Thank you.