Other Parts Discussed in Thread: TUSB1046EVM, TUSB1146, TPS65987D
Hello TI team
- There is a project that use TUSB1046-DCIRNQT,the schematic is referenced TUSB1046EVM. When connect the Displayport and USB3 at the same time, The TUSB1046 registers were configured 0x0A=0x03,0x10=0xAA,0x11=0xAA,0x12=0x02,0x13=0x00,0x20=0xAA,0x21=0x0A,0x22=0x04.The pin25(AUXn) common mode voltage is 1.57V ,and the PIN24(AUXp) common mode voltage is 0.28V. Then pull out the USB3 cable the pin25(AUXn) common mode voltage change to 2.83V, pull in USB3 cable the common mode voltage will drop down to 1.57V again. Can you help me to resolve this issue ?
- When remove the USB3 cable, the device (TUSB1046) can work well 4lane flipping, 4lane not flipping,2lane +USB3 flipping ,2lane +USB3 not flipping .