This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DS of TCA9416 mentions that:
VCCA can be higher than or lower than VCCB. The internal circuitry will select the appropriate supply automatically to correctly support translation.
VCCA can also be the same as VCCB, and the device can be used as a buffer.
In my application VCCA=3.3V and VCCB may be ether 3.3V or 1.8V.
Question: If VCCA=VCCB is it one direction or bidirectional buffer?
Thanks
Vladimir
Thanks Clemens!
Hi Vladimir,
Let us know if you have any more questions.
Regards,
Eric Schott