Good day!
I want to aggregate 8x 640Mbps links on the low speed side into a single 5.12Gbps link on the high speed side. According to table 5.2 and 5.3, my desired 5.12Gbps is slightly out of the supported PLL range. In a demonstration mentioned here (Get Connected: Data aggregation using a general purpose SerDes - Analog - Technical articles - TI E2E support forums), a high speed link at 5.94Gbps (which is also out of the PLL range) has been achieved with a similar TI device. My question is as follows; Can a 5.12Gbps high speed link be achieved with a TLK10081? If not is there an alternative to consider?
With kind regards,
Boris