This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS3301: Increase clamping voltage and VBR

Part Number: TVS3301
Other Parts Discussed in Thread: LM5176, , TSM36A

Hi,

I would like to use this to protect a LM5176. The latter is spec'd to 60V to input range so in terms of clamping voltage the TVS3301 will do a great job. However, I would prefer to allow for an input voltage of 36V +/-5% so Vbr min should be at least 38V. Can you suggest a way to tweak it upward a little?