This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DP83TD510E: Can we use a transformer instead of Capacitor for AC coupling on the MDI side for DP83TD510?

Part Number: DP83TD510E


Yes, transformer can be used for filtering out the DC signal when the data is passing through the MDI side. In fact, we use transformer to filter out the AC signal in the Power over Data Line (PoDL) application. Here are the two way that you can use to filter out the DC signal in the MDI side:

           

--

Regards,

Hillman Lin