Part Number: PCA9306
Other Parts Discussed in Thread: TCA9800, SN74LVC2G66
Hi,
I would like to work with PCA9306 with the same 3.3v on both of his sides (vref1=vref2=3.3V).
I want the device to be like a buffer from my external I2C interface.
i dont have a controller to set the EN pin, can i connect this pin to external PU res?
or should i connect it like in figure 8-6 on datasheet with EN & VREF2 shorted to 200K res to VCC2?