Part Number: TMDS181
Hi,
I'm designing in the TMDS181 as an HDMI sink and I was wondering if my schematic can be reviewed and the following questions answered:
- I have the DDC I2C pulled to 5V on the connector side. The SCL_SNK/SDA_SINK go to 3.3V pins on the FPGA and are pulled up to 3.3V on the FPGA side. Will the 5V pass through the device and present 5V on the SNK sides?
- What should I connect the CEC pin on the HDMI connector?
- Do I need AC coupling caps between the TMDS181 and the FPGA?
Thanks!
John7651.TMDS181.pdf