Part Number: AM26C32
AM26C32IPWR
Hi, Staff
Please let me check the input specification of the device.
Question
1. I don't think the device will be damaged even if the same potential (eg 3V or 5V) is input to 1A (2pin) and 1B (1pin).
2. If the same potential (eg 3V or 5V) is input to 1A (2pin) and 1B (1pin), what kind of potential is output to 1Y (3pin)?
(I think it's indeterminate)
best regards
cafain